AXIS#.TUNING.QUICKTUNE.STATE
Description
Indicates the internal state of the most recent QuickTune process triggered by AXIS#.TUNING.QUICKTUNE.START.
| Value | Description | Cause |
|---|---|---|
| -5 | Set Tuning Error | Tuning parameters were calculated but could not be found in control loops installed on the drive. |
| -4 | Bandwidth Validation Error | Target Bandwidth could not be calculated and AXIS#.TUNING.USERBANDWIDTH was not set. |
| -3 | Inertia Start Error | Inertia measurement could not be started. |
| -2 | Inertia Calculation Error | Error in calculating load inertia. |
| -1 | Error | Unknown error occurred. |
| 0 | Idle | QuickTune process has not been started. |
| 1 | Measuring Inertia | Inertia measurement in progress. |
| 2 | Validating Tuning | Tuning parameter calculation in progress. |
| 3 | Done | QuickTune process completed successfully. |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-02-000 |
- |
General Information
| Type | Read Only |
| Units | N/A |
| Range | -5 to 3 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.TUNING.QUICKTUNE.START |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.TUNING.QUICKTUNE.STATE |
5021h |
06h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5043 |
1 |
5043 (0x13b3) |
AXIS1.TUNING.QUICKTUNE.STATE |
Signed16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.TUNING.QUICKTUNE.STATE |
5043 |
Signed16 |
Read Only |
- |